start_panel_strip |
|
end_panel_strip |
In this section, you will learn about:
Following an EMPro calculation, the results may be reviewed in the Results workspace window. The results that are available in this window depend on the characteristics of the project such as discrete sources, sensors, external excitations, and other project criteria specified in the Simulations workspace window.
This section details the review of results available in this window. Some results will be in the form of numerical values. These are typically single-frequency results performed with a near-zone source. Other results will be displayed in the form of plots. There are several types of plots available to view results based on whether they are time-dependent, frequency-dependent, or angle-dependent. Finally, some results will be available to review as colored field displays. Broadband results collected by Surface sensors and Solid sensors are viewed as individual "Field Snapshots" or "Field Sequences" (strings of snapshots). Three-dimensional far-zone fields may also be available for view depending on simulation criteria.
The Results workspace window stores all of the data collected by the Sensors during the calculation. Once the simulation is queued for calculation, the project will be listed in this window so that the results can be viewed. Additionally, the results of any other saved project can be loaded by pressing the List Project button in the upper-left of the dialog. This makes it possible to view and compare the results of multiple projects without having to load several projects individually. Similarly, the results of any project may be closed by selecting the project and clicking the Unlist Project button.
While the calculation progresses, several options may be selected to control how data is refreshed in the Results workspace window as more and more results become available. The list of results in the workspace window may be manually updated by selecting the Refresh button. The list will be automatically updated if Auto-Update Results check box is selected. This check box will also automatically update plotted data when the specific plot window is opened as the calculation progresses.
It is possible to filter the data within the Results workspace window by searching or by categorizing. The Search box in the top right corner enables you to to search for the name of any field or data visible within the window. The results will automatically appear in the list below.
The user is also able to customize the four columns at the top of the window, which filter data according to the specified categories. The column headings are controlled by right-clicking on any of the current column headings and selecting one of the available categories. Each category is described in the table below.
Data Filter |
Description |
---|---|
Project Id |
Displays the EMPro project ID, which references the location of the loaded project in the file directory. |
Project Name |
Displays the project name indicated by the user. |
Simulation Id |
Displays the simulation ID that refers to the simulation's location in the file directory. |
Simulation Number |
Displays the simulation number that is automatically generated based on how many simulations have been created in a specific project. |
Simulation Name |
Displays the simulation name specified in the Simulations workspace window. |
Run Id |
Displays the run ID which references the location of the run in the file directory. Multiple runs are created in the case that a simulation collects data for more than one variable or location (i.e., during parameter sweeps, multiple ports, etc.). |
Run Number |
Displays the run number. |
Result Type |
Filters results by type. Any of the following results may be viewed depending on the project, simulation criteria, and the type of data that was requested:
|
OUTPUT OBJECT |
Filters results according to its Output Object , which refers to a specific sensor by name. |
DATA TYPE |
Filters results according to the type of sensor that collected the data. The sensor is referenced by its general type, rather than by its user-defined name (Refer to Output Objects for filtering data by sensor name). The following is a comprehensive list of the sensors that may be listed within this filter:
|
Project: Simulation : Run |
Displays the Project, Simulation, and Run name in one column. |
Domain |
Filters data according to Time, Frequency or Discrete Frequencies domains. |
Field Type |
Filters data according to total-field or scattered-field. |
Status |
Displays whether a result is complete or still being calculated while the simulation is running. This status can be refreshed manually by pressing the Refresh button or automatically by selecting Auto-Update Results . |
Misc |
Displays query-specific information. For example, for the circuit component voltage when collecting S-Parameters, it could contain the active port. For S-parameters, it could contain the S number or simply the active port. For System numbers, it could contain the number (such as efficiency) or net input power. |
When a single-frequency calculation has been performed with a near-zone source (voltage or current), parameters such as input impedance, S-parameters, VSWR and the reflection coefficient are displayed as numerical values rather than as line plots since the data only is relevant for the input frequency. Other numerical values are collected by means of a system sensor, which is automatically present in every EMPro project.
Sensor Type |
Time Dependence |
Result Type |
---|---|---|
Port Sensor |
Single-Frequency |
Available Power |
|
|
Current |
|
|
Impedence |
|
|
Input Power |
|
|
Reflection Coefficient |
|
|
S-Parameters |
|
|
Voltage |
|
|
VSWR |
System Sensor |
Single-Frequency |
Dissipated Power |
|
|
Dissipated Power in Non-Tissue |
|
|
Dissipated Power in Tissue |
|
|
Dissipated Power Per Electric Material Component |
|
|
Dissipated Power Per Magnetic Material Component |
|
|
Dissipated Power Per Material |
|
|
Net Available Power |
|
|
Net Feed Loss |
|
|
Net Input Power |
|
|
Radiated Power |
|
|
Radiation Efficiency |
|
|
System Efficiency |
All input impedances are calculated by the ratio of the complex V over complex I for the FDTD mesh edge at the port location. The sign convention is positive for power flow into the antenna or other structure. Thus for a port which delivers power to the antenna, the impedance will have a positive real part, and for a port which absorbs power from the antenna, the impedance will have a negative real part.
When only one active port is present, the feed point impedance at that port is the self-impedance at that port. If more than one port is active, the port impedance values listed represent the ratio of the complex voltage and current at each port including the effects of the sources at all active ports. Thus these impedance values are not the self-impedances at each port, but rather terms of an impedance matrix.
When an S-parameter calculation is made with the steady-state far-zone transformation selected, then both the steady-state antenna data and the S-parameter data will be displayed. This may be useful, for example, when making calculations for a microstrip antenna when both S11 and input impedance are of interest.
The available power is calculated as the total power delivered by the active port or ports into a matched load.
The radiated power is computed as the difference between the total net input power delivered by the active ports and the dissipative losses from conductive materials and resistive loads in inactive ports.
The system efficiency is calculated as the ratio of radiated power to available power. Thus, it includes radiation efficiency and mismatch efficiency.
When viewing single-frequency results collected by the system sensor, the user can specify a scaling factor of the available power to the calculation and determine the scaled result. The absolute input power can be adjusted as desired or an overall scaling can be applied. For example, if the user wanted to know what the output power would have been with an input of one mW, they can enter this value in the available power (will be subject to mismatch loss) or in the net power (after mismatch loss) to see the overall effect. Similarly, any of the output results may be scaled to determine the effect on input and output. Clicking reset will return the values to the un-scaled state.
When making calculations that include the input voltage, current and/or power in the calculation formulas, such as antenna gain or input impedance, the input voltage, current and/or power will be that provided at the terminals of the mesh edge. Referring to the following figure, the impedance at the port would be the (complex) mesh edge voltage V divided by the (complex) mesh edge current I. The complex values would be obtained from an FFT for a broadband calculation or from two samples of the voltage and current (electric and magnetic fields at the port mesh edge) for a sine wave excitation. If the port is delivering power, then the impedance at that port will have a positive real part. If the port is absorbing power, then the impedance at that port will have a negative real part and the input power will be negative. This is determined by the direction of current flow and voltage polarity for the FDTD mesh edge.
Active ports (those with active voltage or current sources) are treated differently than inactive ports for some calculations. For an antenna calculation, the input power to the antenna is the algebraic sum of all powers delivered by active ports. Power absorbed by active ports will not reduce the antenna efficiency; however, power absorbed by inactive ports will reduce antenna efficiency.
To clarify this, consider two different situations. An antenna composed entirely of perfect conductor includes 2 ports, the first containing a 1-V source and a resistor, the second a passive port containing only the resistor. Assuming that some current flows in the passive resistor, the antenna efficiency will be less than 100%. If we repeat the same calculation, but with a 0.00001-V source added to the formerly passive port, and with both sources set active, the antenna efficiency will now be calculated as 100% even though the 0.00001-V source will have negligible effect on the antenna currents and radiation. This discrimination is done so that active ports may utilize lumped circuit elements to match to an antenna without changing the antenna efficiency, impedance, and gain, while passive elements may be added to an antenna with their effects included in the antenna efficiency and gain results.
Similarly, for input impedance calculations, the source resistance, capacitance and inductance values will not be included in the input impedance. For example, the input impedance of an antenna as calculated using EMPro should not change regardless of any changes in the active port components (source/R/L/C). This is as it should be, since the antenna impedance is a function of the antenna geometry/materials and not of how the antenna is fed.
Some results are viewed as 2-D plots. There are three basic categories of plots in EMPro, depending on the X -axis (abscissa) type:
The 2-D plots are viewed by right-clicking on the desired result type in the Results workspace window and selecting Create Line Graph, as seen in the following figure.
Before the graph is displayed, the user has the option of adjusting the graph properties such as the component, data transform, and complex part. The Target Graph option enables you to view and edit plots that were previously created (from the same data selected in the Results window).
The following figure shows samples of the create graph dialog for each plot.
For all calculations, the most important quantities are the time-domain plots of the fields in the problem space. Always perform a quick review of these values to ensure that a calculation has converged. Without convergence, most other results will be meaningless, particularly any plots converted to the frequency domain such as S-parameters or impedance.
Note that input impedance and S-parameters may be plotted in rectangular form vs. frequency or as a Smith chart. |
Sensor Type |
Time Dependence |
Result Type |
---|---|---|
Port Sensor |
Broadband |
Current |
|
|
Impendence |
|
|
Input Power |
|
|
Instantaneous Power |
|
|
Reflection Coefficient |
|
|
S-Parameters |
|
|
VSWR |
Point Sensor/Surface/Volume |
Broadband |
E-Field (E) |
|
|
H-Field (H) |
|
|
B-field (B) |
|
|
Conduction Current (Jc) |
|
|
Poynting Vector (S) |
System Sensor |
Broadband |
Net Feed Loss |
|
|
Net Input Power |
Far Zone Sensor |
Broadband |
Radar Cross Section |
|
|
Gain |
|
|
E-Field (E) |
Far Zone Sensor |
Single-Frequency |
Radar Cross Section |
|
|
Axial Ratio |
|
|
E Theta, E Phi |
|
|
Circular Polarization |
|
|
Ludwig-2 Az, El |
|
|
Ludwig-2 Al, Ep |
|
|
Ludwig-3 |
Far Zone Post Processor |
Single-Frequency |
E-Field (E) |
There are several ways to customize plotted data after it is opened from the Results workspace window. The following sections detail the various tools that are available to modify plotted results.
Keep in mind that the tools available within the plot window depend on the type of graph you are viewing (i.e., XY Plots, Polar Plots, or Smith Charts). |
Select this option to export graphical data point values to a text file in a specified directory.
Select this icon to save an image of the current plot to a specified directory.
Select this tool, and drag the mouse within the plot to pan to the desired view of the plot. Press the |Ctrl| key and drag to pan along the independent axis. Press the |Shift| key and drag to pan along the dependent axis.
Select this tool to zoom-in and to zoom-out of the plot. The mouse wheel as well as the right and left mouse buttons, can be used to perform zoom operations as described below.
Using mouse-wheel:
Roll the center wheel of the mouse forward to zoom-out of both axes simultaneously.
Press |Ctrl| and roll the center wheel forward to zoom-out of the independent axis.
Press |Shift| and roll the center wheel forward to zoom-out of the dependent axis.
Roll the center wheel of the mouse backward to zoom-in to both axes simultaneously.
Press |Ctrl| and roll the center wheel backward to zoom-in to the independent axis.
Press |Shift| and roll the center wheel backward to zoom-in to the dependent axis.
Using mouse buttons:
Right-click and drag the the mouse anywhere in the plot window to zoom-out of both axes simultaneously.
Press |Ctrl| and right-click/drag to zoom-out of the independent axis.
Press |Shift| and and right-click/drag to zoom-out of the dependent axis.
Left\click and drag to define a rectangular view-window in the plot window to zoom-in to both axes.
Press |Ctrl| and left-click/drag to zoom-in to the selected domain of independent axis values.
Press |Shift| and and left-click/drag to zoom-in to the selected range of dependent axis values.
This button toggles the display of the legend within the graph.
The following illustration highlights the three tabs that are available for editing the properties of any graph in EMPro. Each tab is detailed below.
Define the graph name and title as well as the background color of the graph in this tab. A checkbox also toggles the legend display on and off. This tab is displayed in the figure above.
Define the title of the axes and the limits of the axes in this tab. The Auto checkbox may be selected to auto-select these limits.
If a graph only contains continuous data, the X -axis must be specified (this will not happen automatically). |
The Units drop-down menu is used to specify the units and to apply a log scale if necessary.
For certain Smith plots, you will also have the option of modifying the Reference Impedance.
The figure below shows the axes properties editor for a 2-D XY graph.
Define the characteristics of the plotted lines in this tab. A list of every dependent variable is listed with a customizable line color, line width, and line style. Any unwanted variables can also be deleted in this tab.
Select this tool to move, delete, or edit a marker's properties. To move a marker, click on the marker with the selection tool (once selected, it will turn yellow) and roll the mouse-wheel forward or backward to move an attached marker along its plot. Pressing |Ctrl| and rolling the mouse-wheel will speed up the movement of the marker.
To delete any marker, simply select the unwanted marker, right-click and press Delete Marker . All markers may be deleted at one time by right-clicking anywhere in the plot area and choosing Delete All Markers .
To edit a marker's properties, click on the desired marker so that it turns yellow, then right-click and select Marker Properties . A window will appear with several different editing options. The location coordinates of the marker can be adjusted by manually typing in the desired values in the Requested Location section of the dialog box.
If the coordinate box you desire to edit is disabled, select the appropriate option in the Attached plot drop-down menu. |
The marker may also be attached to a particular plot by selecting its name in the Attached Plot drop-down menu and selecting an Interpolation Method for EMPro to use in order to place the point. Depending on this definition, the marker will be shifted to the nearest point on the selected function or linearly interpolated based on the independent axis that is entered by the user in the Requested Location dialog box. Finally, the type of marker can also be redefined in this editor window in the ) Type drop-down list.
Additionally, this tool can be used to move or close the legend in the graphical space. (Any tool, however, can be used to perform this function.)
Select this tool by clicking on its icon or select it from the Markers menu, as shown in below.
Select this tool to mark any point on the plot by clicking on the desired marker location. A marker with the location coordinates will appear above the point, depending on the type of plot:
When the mouse moves close to the plotted curve, it is snapped to the closest location on the interpolated line or sampled point. Holding the |Ctrl| key will disable the snapping action, allowing a point to be placed anywhere. Holding the |Shift| key will snap the marker to sampled points only. Note that markers placed on sampled points are blue, and markers placed on interpolated points are black.
Select this tool to mark the location of a single point by two intersecting cross-hairs. The marker is placed at the right edge of the plot. (Snapping actions are the same as the Point/Tracker Marker described above.)
The following figure shows an XY Plot with a Crosshair Marker (1.8873e-08 s, -6.0381e-06 A) and Point Marker (1.4636e-08 s, 1.0573e-05 A).
The figure below shows a polar graph with a Crosshair Marker along a radius.
The following figure shows a smith graph with a Crosshair Marker along a radius.
Select this tool to place a vertical line that intersects with the X -axis. The marker (Y = constant) will be placed along the top-edge of the plot area. (Snapping actions are the same as the Point/Tracker Marker described above.)
Select this tool to place a horizontal line that intersects with the Y -axis. The marker (X = constant) will be placed along the right-edge of the plot area. (Snapping actions are the same as the Point/Tracker Marker described above.)
The figure below shows a 2-D XY Graph with a Vertical Marker (at X = 1e-08 s) as well as a Horizontal Marker (at Y = 1.5e-05 A).
Colored 3-D field displays may be viewed in slices of the geometry by saving either broadband or single-frequency field quantities. The fields may be viewed in with the geometry (solid or meshed), or by themselves.
Three types of fields may be viewed with the geometry:
Field snapshots are listed in the field control panel as either single slices or as field sequences. The field sequences are movies of the individual slices as the fields progress with time in a particular slice of the geometry. Depending on what was saved, each field snapshot may have electric and magnetic fields, current densities, Poynting vectors stored for each direction (X , Y and Z ) and a display of the combined magnitude. Field snapshots are collected by surface sensors and solid volume sensors for broadband data.
In order to view single-frequency data, the Collect Steady-State Data check box must be checked in the Simulations workspace window (under the Frequencies Of Interest tab). |
Results Plots Available For Each Sensor Type
Sensor Type |
Result Type |
Time Domain |
Discrete-Frequency |
Broadband |
---|---|---|---|---|
Point Sensor |
E-Field (E) |
X |
|
X |
|
H-Field (H) |
X |
|
X |
|
B-field (B) |
X |
|
X |
|
Poynting Vector (S) |
X |
|
X |
|
Conduction Current (Jc) |
X |
|
X |
|
Scattered E |
X |
|
X |
|
Scattered H |
X |
|
X |
|
Scattered B |
X |
|
X |
|
Average Power |
|
|
X |
Surface/Solid Sensor |
E-Field (E) |
X |
X |
|
|
H-Field (H) |
X |
X |
|
|
B-field (B) |
X |
X |
|
|
Conduction Current (Jc) |
X |
X |
|
|
Scattered E |
X |
X |
|
|
Scattered H |
X |
X |
|
|
Scattered B |
X |
X |
|
|
Poynting Vector (S) |
X |
|
|
|
Average Power |
|
X |
|
SAR Sensor |
SAR (Specific Absorption Rate) |
|
X |
|
HAC Sensor |
E-Field (E) |
|
X |
|
|
H-Field (H) |
|
X |
|
|
HAC max E-Field (E) |
|
X |
|
|
HAC max H-Field (H) |
|
X |
|
(Scattered) Electric Fields (E): magnitude, normal, or X , Y or Z components of the (scattered) electric field data at each cell edge.
(Scattered) Magnetic Fields (H): magnitude, normal, or X , Y or Z components of the (scattered) magnetic field data at each cell edge.
(Scattered) Magnetic Flux Density (B): magnitude, normal, or X , Y or Z components of the (scattered) B-field computed from the magnetic fields at each cell edge and the associated permeability for that cell edge.
Average Power Density (SAV): magnitudes of the average power density computed from the electric and magnetic fields at each cell edge.
Conduction Current Magnitude (Jc): conduction current at an electric field cell edge.
SAR (Specific Absorption Rate): computed for each complete cell containing a lossy dielectric with a non-zero material density.
The Results workspace window also displays the data collected within 3-D far-zone fields. Any 3-D far-zone request generated using EMPro's post-processing engine (run separately from the calculation engine) is automatically added once the post-processing is complete. If steady-state far-zone data is enabled for the sensor, the 3-D results will include the E-field and axial ratio in the discrete-frequency domain. Gain or discrete-frequency radar cross section (RCS) will also be available when using a feed or external excitation, respectively.
Note that the polarization (Theta/Phi, Ludwig-2, etc.) is selected through the Setup tab of the Field Editing Toolbar. |
EMPro displays 3-D field data in the Geometry workspace window. The following subsections discuss how to configure and analyze the display, using the Scale Bar, the Field Reader Tool, rescaling, and the field editing toolbar.
The Scale Bar, located at the top of the Geometry workspace window, "paints" the view with a range of colors which correspond to the range of values displayed. By default, the Scale Bar color palette is shown in continuous mode within a default range of values. You can adjust these properties by right-clicking on the scale bar and selecting Discrete Mode, to change the palette to discrete colors, or Automatic Range, to change the range of values to that which is actually present.
There is also a Properties option under the right-click menu. Clicking this will bring up the Scale Bar Editor. Using this editor, you can manually set the Scale Bar limits, units and colors to your preference. Take note of several settings that may not be intuitive for the first-time user:
The following two figures show the Scale Bar Editor, and the Scale Bar_ with the Field Reader tool.
The Field Reader Tool is located in the toolbar to the right of the Geometry workspace simulation space. After selecting this icon, wheel the mouse over the geometry object to identify its field values. A marker in the Scale Bar will display the nearest known field value to the location of the mouse. This location is represented by a small dot on the screen.
In the Results workspace window, filter the results by the output object System. Double-clicking on results such as Dissipated Power or System Efficiency will open the System Sensor Output dialog box. Changing any value in this table will rescale the other values shown.
The Show Scaled Values box must be selected to enable editing in the System Sensor Output dialog box. |
Located at the bottom of the Geometry workspace window, the field editing toolbar is used to configure the properties of the view. In the upper-left corner of this toolbar, a drop-down list will display any view that you have opened from the Results window. You can use the Hide Others and Unload buttons to single out certain view(s) if necessary. The following figure shows a drop-down list of such results in the field editing toolbar.
The tabs and configuration options below will change depending on the active view. A comprehensive list of the available options are described below.
There are two main configurations for the Setup tab, depending on the type of sensor you are evaluating.
This tab is available when viewing an SAR, Solid, or Volume sensor. Configure the settings here to "play through" a simulation.
The Rotations tab, shown in Figure 13.20, oers several operations to adjust the orientation of the far-zone results by setting the Up Vector of the view. Changing the Up Vector (which is the Z-axis by default), will set the reference point for the spherical coordinate systems (e.g., theta/phi, alpha/epsilon, etc.) This affects field plots of single polarization components, partial power effciency and power computations, mean eective gain computations, and antenna diversity. This is useful in
cases where the geometry is aligned with an axis of the computation grid, but the real-world position of the geometry is not axis-aligned.
The PDF tab controls the settings used in the computation of mean eective gain and antenna diversity far zone results. The following illustration shows the PDF tab.
theta0radians phi0radians pdfAtTheta0Phi0
theta0radians phi1radians pdfAtTheta0Phi1
...
theta0radians phi19radians pdfAtTheta0Phi19
theta1radians phi0radians pdfAtTheta1Phi0
...
theta9radians phi19radians pdfAtTheta9Phi19
There are two main configurations for the Statistics tab, depending on the type of sensor you are evaluating.
Keep in mind that not all fields listed will be available for every view. |
The next figure shows the Statistics tab for a far-zone sensor configuration.
When selected, Power/Efficiency gives the user the option of choosing from among the following radiation patterns:
• Full Pattern - specifies the use of a full far zone sphere.
• Upper Hemisphere - specifies the use of theta = [0, 90o] and phi = [0, 360o].
• Open Sky - specifies the use of theta = [0, 80o] and phi = [0, 360o].
• Partial Pattern - enables you to specify an arbitrary solid angle. These angles are defined relative to the coordinate system defined under Rotations.
Each pattern will display its statistics to the right. In the case of Partial Pattern, the user can redefine the min and max values of Phi and Theta by typing them in to the corresponding boxes. The statistics will update accordingly.
The Other Statistics option presents a list of additional statistics.
statistics
The next illustration shows the Statistics tab for an SAR sensor configuration.
This tab is available when looking at SAR data for both the SAR Sensor and the SAR Averaging Sensor. The following figure displays the dialog that appears when the View All SAR Stats button is pressed.
For more information on rescaling values in the System Sensor Output dialog, refer to Rescaling. |
The Diversity tab is used to compute antenna diversity metrics between two far zone patterns. To perform the diversity computations, you must load the data for both far zone patterns in the Results workspace. Then go to the diversity tab for one of the two patterns. The following figure shows the Diversity tab.
Note that the XPD and PDF settings under the PDF tab impact this computation, as well as the settings under the Rotations tab. |
This tab, as the name suggests, is only available when viewing (HAC) sensors.
An example of this format is as follows:
! This is a comment
Band 1 Name;0.85;0.9;0.8;-5; 0
Band 2 Name; 1.0; 0.92; 0.33; 0; 1
Post-processing gives the user the option of running additional computations after the calculation engine run is finished to save certain results to disk. Two types of post-processing are available.
Far-zone post-processing is enabled by checking the Save Data for Post-simulation Far Zone Steady-state Processing box under the Frequencies of Interest: Data Storage tab of the Simulations workspace window. When this configuration is set, there will be an entry for Raw Steady-State Far Zone Data in the Results workspace window. Double-clicking this entry will enable you define a new far zone geometry at which the steady-state far zone pattern will be computed. Edit the geometry exactly as you would edit a far zone sensor. When you click Done in the far zone sensor editor, the computation of the far zone pattern will begin. Once complete, you can find a new result in the Results workspace window which corresponds to the newly defined far zone pattern.
Right-clicking on any Raw SAR Sensor entry in the Results workspace window will show an option in the context menu to Postprocess Results. This enables you to perform SAR averaging. Edit the geometry and averaging parameters exactly as you would in the SAR Averaging Sensor editor. Once you click Done in the editor, you will be given the option to automatically run the post-processor. If you say yes, the post-processing operation is queued as if you had created a new simulation. Otherwise, you will have to do the post-processing run manually. Once the SAR averaging is complete, new SAR average data will appear in the Results workspace window.