The first component, which is referred to as "ADS-FEM Integration Update," needs to be installed on top of the existing ADS2009U1 installation.
The second component, which is referred to as "FEM Simulator Update (2010.07)," describes the fix which needs to be installed separately from ADS2009U1.
These two components can be installed in any order.
If you have already installed “ADS-FEM Integration Update” while using previous ”FEM Simulator Update (2010.07)” based on FEM engine technology upgrade from EMPro 2009, Step 1 above is not required.
The following areas are addressed in this upgrade:
Various meshing issues fixed (with upgrade to EMPro 2010.07 meshing).
New mechanism to reduce Port parasitics effects for internal ports.
3D stereo view with nVidia glasses.
64-bit mesher, 64-bit visualization on Linux, 64bit Far field on all platforms.
Fix for bond wire profile for low-clearance bond wires.