PathSelect2 (Coordinated set of Single Pole Double Throw Static Switches)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
State |
State of switch: 0=lower path, 1=upper path |
None |
0 |
Notes/Equations
- This model defines a pair of coordinated static single pole double throw switches that enables connectivity for one of two paths with ideal isolation between the paths.
- This component uses internal models for SPDT_Static. The schematic design is shown here:
- When State=0, connectivity occurs from port 1 to port 2 to port 3 to port 6.
- When State=1, connectivity occurs from port 1 to port 4 to port 5 to port 6.
- When using this device in a transient simulation, the switch setting must be constant.
- An example demonstrating this model is located in ADS; access the design from the ADS Main window: File > Example Project > Tutorial > RF_Budget_Examples_prj ; see Budget_Mixer.dsn .