Comparator (Comparator)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
Vlow |
Lower threshold voltage |
V |
0.25 |
Vhigh |
Upper threshold voltage |
V |
0.75 |
Notes/Equations
- Comparator outputs a 1V signal whenever the baseband portion of the input signal is between the two threshold voltages. Input impedance is infinite; output impedance is fixed at 0.1 Ohm; and, there is a fixed delay of one timestep.
- If the baseband portion of Vin is greater than Vlow and less than Vhigh, then the output voltage at the next time sample is 1.0V; otherwise, the output is 0.0V.
- This model works in transient and circuit envelope simulation.