IQ_ModTuned (I/Q Modulator, Tuned)
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
Fnom |
Nominal input frequency |
GHz |
1 |
Rout |
Output resistance |
Ohm |
50 |
Notes/Equations
- This is a tuned modulator that selects the input harmonic defined by the specified Fnom frequency and modulates it according to the I (in-phase) and Q (quadrature) modulation inputs.
If there is no analysis harmonic frequency close enough to the Fnom frequency, a warning is issued and the output is 0. All three input impedances are infinite; output impedance is set by Rout, and is limited to a minimum value of 0.1 Ohm. The open circuit output voltage is defined by
where
k represents the value at the analysis harmonic frequency closest to the Fnom value
0 represents the baseband component of the two modulation input voltages. - The RF carrier is injected at pin 1; I data is injected at pin 3; Q data is injected at pin 4. The resulting modulated signal is present at pin 2. The RF carrier should be a frequency-domain source; the modulating signals should be a time-domain source.
- This model will not function as a phase modulator in transient and baseband envelope simulation because of the use of the complex j operator.
- Both AM and PM modulation can be generated.