AmplifierVC (Ideal Voltage-Controlled Amplifier)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
Gain |
Gain as a function of control voltage (_v3) |
dB/V |
(30 − 15 × _v3) |
Rout |
Output resistance |
Ohm |
50 |
Range of Usage
Rout > 0
Notes/Equations
- AmplifierVC is an ideal voltage controlled amplifier. The impedance for its input and control port is infinite; its output impedance is Rout.
- An equation is used to describe Gain as a function of the control voltage at port 3: _V3. The default equation is Gain = 30 − 15 × _V3.