VMult (Voltage Multiplier)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
R1 |
Reference resistance for port 1 |
Ohm |
50 |
R2 |
Reference resistance for port 2 |
Ohm |
50 |
R3 |
Reference resistance for port 3 |
Ohm |
50 |
L31 |
Loss in dB, pin 1 to pin 3; for linear analysis only |
dB |
0 |
L32 |
Loss in dB, pin 2 to pin 3; for linear analysis only |
dB |
0 |
Linear |
Use linear analysis mode: yes or no |
None |
no |
Notes/Equations
- VMult uses reference input and output impedances. Its output voltage is equal to the product of its two input voltages.
- If Linear is set to yes,
A31 and A32 are the L31 and L32 losses converted from dB to regular values.
If Linear is set to no, V3 is formed from V1 and V2 through an ideal mixing process; for information on this process refer to the SDD example, Ideal Mixer.