AmplifierP2D_Setup (Extractor Component for AmplifierP2D)
Symbol
Available in ADS
Parameters
Name | Description | Unit | Default |
---|---|---|---|
Filename | Name of P2D file to be generated by extractor | None | p2dfile.p2d |
Order | Order for Harmonic Balance simulation inside extractor; must be an integer greater than 0 | None | 10 |
Freq_Start | Start value for sweep of large-signal frequencies; must be a positive real number | GHz | 1.0 |
Freq_Stop | Stop value for sweep of large-signal frequencies; must be a positive real number | GHz | 2.0 |
Freq_Step † | Interval for linear sweep of large-signal frequencies; must be a positive real number | GHz | 0.1 |
Pin_Start | Start value for sweep of large-signal input power; must be a real number | dBm | −10.0 |
Pin_Stop | Stop value for sweep of large-signal input power; must be a real number | dBm | 15.0 |
Pin_Step † | Interval for linear sweep of large-signal input power; must be a positive real number | dB | 5.0 |
SSFreq_Start †† | Start value for sweep of small-signal frequencies; must be a positive real number if specified | ||
SSFreq_Stop †† | Stop value for sweep of small-signal frequencies; must be a positive real number if specified | ||
SSFreq_Step † , †† | Interval for linear sweep of small-signal frequencies; must be a positive real number if specified | ||
† Only linear sweeps using intervals of Freq_Step, Pin_Step, SSFreq_Step are permitted frequency and power extractions using the AmplifierP2D_extractor. †† Small-signal frequency settings, if left unspecified, will default to large-signal frequency specifications. The default behavior of this component is to enforce SSFreq_Start <= Freq_Start, SSFreq_Stop >= Freq_Stop and SSFreq_Step <= Freq_Step. Violations of this will result in internal correction with warning messages being reported to the simulator log window. Refer to note 4 for modifying this default behavior. |
Notes/Equations
- AmplifierP2D_Setup is a data file extractor component used to create multi-dimensional behavioral profiles of a circuit level amplifier in the P2D format. The use of this component is highlighted in the design CKT_P2D_extraction.dsn of the example project AmpP2D_prj.
- AmplifierP2D_Setup can be pushed into for a view of the implementation. If necessary, the component can be copied and modified to suit individual needs.
- AmplifierP2D_Setup performs a linear swept input frequency over linear swept input power P2D (Harmonic Balance) simulation of a circuit-level amplifier and generates a P2D file for subsequent use by the data-based system model AmplifierP2D. The Freq_ and Pin_ parameters regulate the large-signal frequency and input power sweeps, respectively.
- The small-signal frequency sweep can be specified independently of the large- signal frequency sweep using SSFreq_ parameters. When unspecified, these values internally default to large-signal values. When specified in violation of the rule that SSFreq_Start <= Freq_Start, SSFreq_Stop >= Freq_Stop and SSFreq_Step <= Freq_Step, this rule is imposed internally during simulation and warning messages appear in the simulator log window. This ensures the small-signal frequency sweep spans the large-signal frequency sweep and is at least as finely grained. This is the coarsest granularity for reliable modeling using the AmplifierP2D data model.
- In order for AmplifierP2D to produce an accurate model of the circuit-level amplifier characterized via AmplifierP2D_Setup, the Order parameter for AmplifierP2D_Setup must be large enough to prevent aliasing of higher-order frequency components. Because the AmplifierP2D data model reads and operates primarily on its assigned fundamental frequency, it is important to provide an accurate estimate of the fundamental response at the circuit level amplifier output. Therefore, it is important to use a large order of harmonics in AmplifierP2D_Setup to reconstruct the fundamental accurately during data modeling. The recommended value is 5 for mildly non-linear circuits and 11-15 for highly non-linear circuits.
- For information regarding the P2D data format, refer to PDF Format. Multi-dimensional P2D files may be generated by simply placing a chain of ParamSweep controllers above the AmplifierP2D_Setup instance and assigning the lowest sweep to have SimInstance[1]="Xi1.HB" where "Xi" is the instance name of the P2D extractor and HB1 is the default name of the P2D controller within its subcircuit.