Pad (Pi or Tee Format)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
NetType |
Network type: Pi or Tee |
None |
Pi |
Loss |
Attenuation |
dB |
0 |
R1 |
Reference resistance for port 1 |
Ohm |
50 |
R2 |
Reference resistance for port 2 |
Ohm |
50 |
Temp |
Temperature |
°C |
None |
CheckPassivity |
Check passivity flag: if set to yes, a passivity check is performed and a warning is output if the device is not passive; if set to no, a passivity check is not performed. |
None |
yes |
Range of Usage
R1 > 0
R2 > 0
Notes/Equations
- This 2-port component provides a:
- Match to resistance R1 at port 1 when port 2 is terminated in R2
- Match to R2 at port 2 when port 1 is terminated in R1
- Desired attenuation, DB
- Resistive networks can achieve simultaneous match at input and output if the insertion loss factor A exceeds a minimum value given by
where:
DBMIN = 10 × log10(AMIN) - The values shown in the Pi network equivalent circuit are given by:
The values shown in the Tee network circuits are given by
Equivalent Circuit