Circulator (Ideal 3-Port Circulator)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
F1 |
First frequency breakpoint |
|
|
F2 |
Second frequency breakpoint |
|
|
F3 |
Third frequency breakpoint |
|
|
Loss1 |
Attenuation for frequencies ≤ F1 |
dB |
0 |
Loss2 |
Attenuation for F1< frequency ≤ F2 |
dB |
0 |
Loss3 |
Attenuation for F2 > frequency ≤ F3 |
dB |
0 |
Loss4 |
Attenuation for frequencies > F3 |
dB |
0 |
VSWR1 |
Voltage standing wave ratio at both ports for frequencies ≤ F1 |
None |
1 |
VSWR2 |
Voltage standing wave ratio at both ports for frequencies > F1, ≤ F2 |
None |
1 |
VSWR3 |
Voltage standing wave ratio at both ports for frequencies > F2, ≤ F3 |
None |
1 |
VSWR4 |
Voltage standing wave ratio at both ports for frequencies > F3 |
None |
1 |
Isolat |
Isolation |
dB |
100 |
Z1 |
Reference impedance for port 1 |
|
|
Z2 |
Reference impedance for port 2 |
|
|
Z3 |
Reference impedance for port 3 |
|
|
Temp |
Temperature |
°C |
None |
CheckPassivity |
Check passivity flag: if set to yes, a passivity check is performed and a warning is output if the device is not passive; if set to no, a passivity check is not performed. |
None |
yes |
Notes/Equations
- Up to three frequency breakpoints can be used to define four bands. Each band will have a different Loss# and VSWR#. If no frequencies are specified, then this model is frequency independent and only uses Loss1 and VSWR1.
- A loss is modeled regardless of the sign of the Loss parameter value.
- All ports have the same VSWR.
- Isolation is constant across all frequency bands.
- The 3 × 3 S-matrix for Circulator is described by