RF_RX_SML (RF Receiver)
Symbol
Available in ADS
Parameters
Name |
Description |
Units |
Default |
---|---|---|---|
RX_AntTemp |
Receiving antenna noise temperature |
None |
150 |
RX_Gain |
Receiver gain |
dB |
50 |
RX_NF |
Receiver noise figure |
dB |
5 |
RF_Freq |
RF frequency |
MHz |
900 |
RF_BW |
RF bandwidth |
MHz |
25 |
IF_Freq1 |
First IF frequency |
MHz |
100 |
IF_Freq2 |
Second IF frequency |
kHz |
400 |
IF_BW |
IF bandwidth |
kHz |
30 |
IP3in |
Receiver input IP3 |
dBm |
−25 |
RIn |
Input resistance |
Ohm |
50 |
ROut |
Output resistance |
Ohm |
50 |
Notes/Equations
- This is a super-heterodyne RF receiver subsystem. Input is an RF signal; output is an IF signal. Three CW spurs are combined with the input RF signal to simulate the receiver interference performance.
This subnetwork is provided for easy inclusion of an RF receiver in an ADS Ptolemy Envelope co-simulation.