Advanced Design System 2020 Release Notes
For general information about Advanced Design System (ADS), visit ADS webpage at http://www.keysight.com/find/eesof-ads.
Starting ADS 2020 release, the Linux system requirements have been updated: Few ADS features will not work properly, in case you have installed lower patch versions than the above-recommended versions. For more information, refer to Supported Platforms.
Feature Updates
- Design and Technology Management
- Design Editing
- Circuit Simulation
- HSD Design
- EM Simulation
- PDK Validator
- Verification Test Bench (VTB)
- Examples
- Licensing
- Documentation
Design and Technology Management
General
Improved Reference Searching and Display. "Explain" references describes and shows reference information to explain relationships in your libraries and designs. See References and Dependents.
- Improved Data file support in Library View and Copy Files.
- Data Display
- Added Data Display Expression Manager to edit, find and/or replace equations and export measurement equations.
- Find equation and trace dependents in Data Display. For more information, see Finding Dependent Equations.
- Data Display Performance Improvements.
- Datalink (Python Interface)
- Datalink functions are available in measurement equations. For more information, see Adding Datalink Function in ADS.
Design Editing
- Layout Constraints Database is a central location to define constraints on layout designs, such as trace widths, via start and stop layers, and routing clearances. The initial release of the layout constraints database implements two types of constraints: Clearance constraints and Via constraints. For more information, see Layout Constraints Database.
Define and Insert PCB Vias and Pads using Padstack Templates.
Circuit Simulation
General
- Loop Gain based stability analysis. For more information, see WSProbe (Winslow Stability Probe).
- Support SystemVue 2018 update1.0 and latest 5GNR for modulated signals. For more information, see Verification Test Bench (VTB).
- Direct EVM computations without dataflow simulator. For more information, see EVM computations.
Simulated annealing optimization supports discrete variables and has improved performance. For more information, see Simulated Annealing Optimizer.
Electrothermal
- Using Design with Non-Synchronized Hierarchy. For more information, see Using Design with Non-Synchronized Hierarchy.
- Electrothermal controller default values can be pre-configured using the eth.cfg file. For more information, see Setting Defaults for ETH Controller .
Beta – ETH Circuit Envelope simulation allows the specification of an arbitrary synchronization time schedule (that is arbitrary time steps as a function of time) in contrast to the preceding uniform or logarithmic progressions.
For more details on use of arbitrary timestep, see Parameters in Simulator timestep Section.
- NXP SiMKit Models
- The models have been updated to SiMKit Release, and these are now the default.
For more information, including supported device versions, see Devices and Models, NXP SiMKit.
- The models have been updated to SiMKit Release, and these are now the default.
HSD Design
General
- Queue Manager (QM) to manage test bench/benchs in ADS. For more information, see Queue Manager.
SerDes
CTLE Visualizer. For more information, see CTLE Equalization Parameters.
Easier CTLE setup with provided presets for OIF CEI-28G. CEI-56G-VSR, IEEE 802.2bs CDAUI8, PCIe and USB Gen3.
Display frequency response, magnitude and phase.
Support user provided presets.
MIPI C-PHY Receiver enhancement with CTLE. For more information, see Rx_Cphy (MIPI C-PHY Receiver).
FlexDCA_Probe connection enhancement for remote H/W and remote PC. For more information, see FlexDCA Probe.
COM (Channel Operating Margin). For more information, see Support of Matlab runtime.
Linux Matlab runtime support.
COM 2.6 and Matlab R2018b support.
- Smart Eye Probe: Multilane support with triggered eye diagram. For more information, see Smart Eye Probe.
- DDR/Memory
- DDRSetup for Memory Designer
- Improvements in setup SIPro simulations for DDR design
- Improvements in use flow SIPro->Memory Designer
DDR Package components to specify packages that are not part of an IBIS file. For more information, see DDR Package.
- DDRSetup for Memory Designer
- EM-SI/EM-PI
- Via Designer
- multi-feed vias
- micro vias and staggered vias
- export to layout
- export to EMPro
- custom stitching via layers
- Parallel simulation jobs for SIPro
- local parallel simulations
- parallel simulation jobs on cluster
PCB Import generates a Model Map File
Model Map File generates Schematics and Symbols for user selected components
Model Map File can be edited to point to vendor libraries and custom models
PIPro DeCap Optimization with Lib Cell and SnP Components
PIPro Multi-Pin Splitting from 1 Sink to Multiple Sink Pin Pairs
PIPro Multi-Pin Accuracy Improvements
Equal Current and Equal Voltage now result in lower impedance with improved distribution of currents.
ADFI Export for Package Import into PIPro
Custom ADFI setting for exporting packages from Cadence SiP and MCM for use in SIPro/PIPro.
PIPro Improved multi-pin grouping and ungrouping for Current Mode and Voltage Mode AC EM Model solutions.
- Faster rendering of large designs during rotate/pan/zoom. During these operations, reduced geometry detail is rendered to preserve an acceptable frame rate.
- Via Designer
For more information, see SIPro and PIPro.
EM Simulation
RFPro
- The User-Defined EM Extraction analysis allows to EM-simulate a combination of selected nets and components of a large design.
- Simulate frequencies in parallel with FEM (on the local host or submitted to a cluster queue) and Momentum (only supported for jobs submitted to a cluster queue). Specify the number of parallel jobs in the Analysis → Options → Resources tab.
- LTD substrate files are available for selection when creating a new RFPro view.
- Specify the layer purposes to be excluded or included when opening a layout in RFPro in the substrate editor (.subst or .ltd).
- Context menus have been added to pin(s) allowing to create a virtual pin on a layer.
- The S-Parameter → Save As dialog has a new flag to open a Data Display window after exporting the S-parameters to a dataset.
- Create Script context menu option has been added to analyses allowing you to transfer an analysis setup to another view. The script can also serve as a starting point for learning how to define an analysis through a python script.
- Faster rendering of large designs during rotate/pan/zoom. During these operations, a reduced geometry detail is rendered to preserve an acceptable frame rate.
- Preview the next generation FEM simulator by setting the environment variable RFPRO_FEM_GENERATION=2. The 'pilot' code in the ADS 2020 release brings much faster pre-processing of (multi-technology) designs and a 'Mesh Domain Optimization' simulator option. The new flow can be used as an alternative to the default (RFPRO_FEM_GENERATION=1) FEM simulator.
- ADS 2020 release is the last release with Python 2.7 as Python 2.7 is reaching its end-of-life. ADS 2021 release is planned to use Python 3.7. A pilot release with Python 3.7 is available for download. Contact Technical Support for further guidance.
- ADS 2020 release is the last release to support 32 bits version of Cadence Virtuoso. ADS 2021 is planned to support only the 64 bits versions of Cadence Virtuoso.
- EM Setup
- An issue has been addressed in the EM Setup based interoperable EM-Cosimulation flow. The view generation failed when 1x1 OA via arrays are present in the layout.
- An issue has been addressed in the EM Setup based interoperable EM-Cosimulation flow. The view generation failed when 1x1 OA via arrays are present in the layout.
- FEM
Mesh generation performance and robustness improvements.
- Increased robustness of the parallel frequency sweep.
- Queue resource mapping tied to master/mesh/solve phase with 'sitecluster'.
- Momentum
- Refinement of the AC-behavior of the new conductor loss model introduced in ADS 2019. When cumulating edge mesh and thick metals, it could lead to an overestimation of the resistance with increasing frequency. This issue has been addressed. The workaround of setting MOM3D_USE_LOCALTHICKNESS = 0 is no longer recommended.
Power Electronics
Power Electronics Professional (PEPro)
- Next generation post-layout EM-circuit co-simulation platform for switched-mode power supply (SMPS) designs.
- Automatic optimum settings of EM and Transient/Convolution simulation controllers for SMPS design.
- Pre-built testbenches for Voltage Spikes and Conducted EMI analyses.
For more information, see PEPro.
PDK Validator
Process Design Kit (PDK) Validator provides automation technology for delivering high quality, fully enabled ADS PDKs.
- Verify PDKs with a new ADS release
- Enable features (DRC, LVS)
For more information, see PDK Validator.
Design Rule Check (DRC)
Assura DRC
Rule Categories
- Improved support for rule files with switches. Switches are now automatically detected.
ADS DRC
Capacity and Performance
- Improved support for large rule files with many input layers.
- Improved efficiency for the dve_quadout() command
- Impacts rules that perform an external clearance rule and then extract quadrilaterals from the selected edges. Can result in a significant performance improvement for designs that contain circles or traces with round end type.
DRC Documentation
- 100+ examples of how to write rules.
- Find information easily. Browse to the Rules using the Navigation panel.
- Writing Design Rules provides sample rules files that illustrate rule categories and process variants.
Rules syntax updated to show all supported parameters. For example, Polygon Selection rules support a message parameter which provides a simpler rules syntax.
For more information. see Design Rule Check (DRC).
Design Kits
- Updated the Si-RFIC PDK Model Include Utility for the following:
- “None” scenario has been added as one of the default scenarios.
- Updated the Model Include Component, you can now invoke the settings dialog box from the component itself.
- Removed the following legacy and old ADS demo kits from ADS 2020 installer:
- DemoKit
- DemoKit_V3
- SampleKit
- eesofDemoKit
- Updated the ADS Non-Linear Demo Kit for the following:
- All the DSN references have been removed from the design kit.
- A new substrate "demo_modified.subst" is added with practical values of material conductivities to synthesize more realistic inductors.
- CNEX Component Definitions are added to support Calibre LVS and Assura LVS.
Verification Test Bench (VTB)
ADS 2019 only supports import of Custom VTB (SystemVue workspace) created using SystemVue 2018 and SystemVue 2018 Update 0.1.
Examples
- All the newly added examples are searchable using the Example Search dialog box.
For more information, see Working with Example Workspaces.
Licensing
- ADS 2020 requires: a) the version 2019.02 of the EEsof EDA licensing software, b) a minimum code-word version 2019.02 or above, and c) the licensing server software, lmgrd and agileesofd, to be upgraded to at least the same versions as what are included in EEsof EDA Licensing software 2019.02. ADS All-Versions will not start if any of these requirements is not met. Refer to the License Codeword Version Compatibility Table.
- In the EEsof EDA License Tools version 2019.02, licensing vendor daemon (agileesofd) is integrated with FlexNet FNP 11.13.1.4 version (Windows) and FlexNet FNP 11.13.1.3 version (Linux) of FlexNet license manager daemon (lmgrd). For the Windows platform, ADS installer will automatically set up these two new license server daemons by default for the local node-locked license users; for the Linux platform, you need to follow the Linux Licensing Setup instruction to complete the licensing configuration process. For more details, refer to Licensing (For Administrators).
Documentation
Starting with the 2020 release, the online help gets a new user interface. The new UI improves overall online help usability by providing the following key benefits in addition to several other minor benefits:
- Table of Contents Sidebar: Displays collapsible Table of Contents for the entire documentation. The left-double-arrow icon collapses the sidebar, and the right-double-arrow icon displays the sidebar back again.
- PDF Button: Allows you to instantly generate PDFs of the latest documentation anytime, including current page’s children pages. Currently, the PDF generation option is available only for ADS 2020 release. For other releases, you can switch to their Printing Manuals page and download the existing PDFs like earlier. Note that with the introduction of PDF generation feature, the Printing Manuals page will not be available from next release onward.
- Product Release Switcher: Allows you to view the current page in other supported releases listed in the drop-down menu. Once you select a release from the drop-down menu, the current page is updated to show the content applicable to the selected release. The Table of Contents is updated as well. With this, you bookmark URL of only one release and then switch to other releases from this drop-down menu.
- Latest Documentation: The documentation available in the new UI is always kept updated for all supported releases. These updates are available to you as soon as they happen at our end. This provides you 24x7 access to the most recent and technically accurate documentation.
For more details, see How to Use Online Help.
Known Issues
Design and Technology Management
Using ADS 2020 with pycell studio 2018 (PyCell Studio Packages: Release O-2018.09) might prompt you an OA version mismatch warning message on the linux terminal. However, there is no impact on the iPDK flow in ADS.
Linux terminal message:
Requested minor API version '518', which is supported by OpenAccess build '22.50.030' is newer than the minor API version '514' of the shared library of OpenAccess build '22.50.043'.The Express Pcell plugin that comes with Virtuoso IC version 6.1.8 does not work with ADS 2020 due to an OpenAccess version mismatch.
Workaround: When running ADS 2020, set the LD_LIBRARY_PATH environment variable path to point to the directory from IC version 6.1.7.AEL constants are protected and should not be modified in any DDS expressions. An AEL error will be issued in case an attempt to modify an AEL constant occurs.
- Python Datalink
- When using Connection Expert 2019 connected to Lan Instruments, there may be error messages during dl_visa_query() and dl_visa_write().
- Exceed on Demand: Note that in some cases, EoD settings may need to be configured to properly display Spyder. Please contact your EoD support representative for additional guidance.
Design Editing
- Designs created using Smart Mount for Multi-Technology feature cannot be used to run an electrothermal simulation.
Design Guide
- Simulating the "1_Sim_CA" design in the DDR4 CTB design guide prompts the netlist error.
Workaround: Open the schematic design "PatternGen_CA_Continuous" and arrange the pin numbers in order. Simulating of schematics in the HDMI_Link_Simulation design guide prompt the netlist error.
Workaround: Open the schematic design “HDMI_Diff_RX” and arrange the pin numbers order in order.
Circuit Simulation
General
Simulation Manager may not work on Windows and throw exceptions for some designs.
ADS 2019 will not be compatible with Verilog-A files, which have been encrypted before ADS 2019. There is no change for non-encrypted Verilog-A files.
Electrothermal
You may not be able to start a Transient/Envelope Electro-Thermal (ETH) simulation only when the same testbench is open in the viewer of Transient/Envelope thermal results. You need to close the viewer before launching a Transient/Envelope ETH simulation.
The electrothermal simulation will not run on designs created using Smart Mount for Multi-Technology feature.
Paths set while configuring the ETH controller may need to be updated when the workspace is moved across operating systems.
On a fresh Linux machine, electrothermal simulation fails with the following error message:
Heatwave returned an unknown error code 127.
Workaround: The error could be due to missing packages, for example, libpng12. Verify your system meets the requirements using the linux_sys_check.sh script. For more information, see Checking Installed RPM Files and the Operating System Version.
If you get licensing errors while running thermal simulation, you may need the following workaround.
Workaround: Rename the file$HOME/.eesofrc
. For example,$HOME/.eesofrc-orig
.Electrothermal does not support remote simulation, batch simulation, Monte Carlo, tuning, Optimization, and Measurement Equations. Also, you cannot sweep directly on the DC controller.
All libraries referenced in a layout should use the same layout resolution, namely the OA database units (DBU) per user unit (UU).
You cannot run both a transient and envelope simulation on the same design from one testbench.
The calculation of power dissipation from passive components other than resistors may not be correct in harmonic balance simulations.
Electrothermal does not support the transient or envelope simulation that is controlled by a ParamSweep.
If you get "Maximum timestep reduced to half of shortest transmission line delay " warning, it can lead to transient simulation to not converge
Workaround: Unselect "Limit timestep for Transmission Line" option on Time Setup tab of Tran component to get it work.On Linux, if you specify the THERMAL_DIRECTORY variable in eesof_lib.cfg file using backward slash (..\thermal), the thermal simulation does not run properly.
Workaround: Specify the THERMAL_DIRECTORY variable using forward slash (../thermal) instead of backward slash.The ETH viewer does not support 4K displays. A few instances of text and icons may appear distorted.
You receive an error message in substrate editor that you cannot use the same layer number more than once. You can safely ignore this error during thermal technology export.
On a fresh Windows 10 system, Electrothermal simulation terminates with an error.
Workaround: Install the following Microsoft Visual C++ runtime components:http://www.microsoft.com/en-in/download/details.aspx?id=30679
https://www.microsoft.com/en-in/download/details.aspx?id=5555
DDR Design
You receive an error message to check port numbering when performing simulation with SnP component for differential configuration.
Workaround: Select the first option in Pin Configuration for the SnP component.
HSD Design
- SerDes
You receive an error message when runtime libraries for some of the ADS example ibs files (for old AMI models) are unable to get installed automatically during the ADS install.
The error appears eventhough the ibs file is supported on specific platform.
Workaround: Microsoft Visual C++ 2010 runtime library is required to run the dll files. Download the following library if it is not installed:https://www.microsoft.com/en-us/download/details.aspx?id=14632
- EM-SI/EM-PI
- SIPro/PIPro, Via Designer
- On Windows 10 with Intel HD graphics, Via Designer may show an error message ‘Failed to use connection between ADS and Via Designer’. This has been isolated to the latest release of Intel HD Graphics drivers (23.xx.xx.xxxx).
Workaround: Downgrading graphics driver to the previous recommended driver resolves this issue (e.g. 22.20.16.4836,A05). - DirectX 9 as graphics driver is no longer supported. DirectX 11 is thus be used by default. Run "diagdx" to verify which DirectX version is supported on your system.
- On Windows 10 with Intel HD graphics, Via Designer may show an error message ‘Failed to use connection between ADS and Via Designer’. This has been isolated to the latest release of Intel HD Graphics drivers (23.xx.xx.xxxx).
- SIPro/PIPro
- ADS 2020 is not compatible with the latest available Samsung component models released in June 2018. The support for the component models is planned to be added in an upcoming update release.
- Simulation failure when using components with S-parameter models or for which the model is defined using a lib/cel/view in case the Updating model does not require new simulation is not set. As a workaround, turn on the option. For PI-AC simulations, the options is turned on by default, for SIPro, this needs to be turned on explicitly.
If you run SIPro/PIPro on a fresh machine with Suse 11 installed, you may encounter the critical error, "EMPro exited unexpectedly during execution."
Workaround: Run the following commands:cd $HPEESOF_DIR/fem/2020.00/linux_x86_64/bin
./startempro --personality=sipi --driver=x11
Ignore any license related error messages that may show up on executing these commands. These driver settings are saved for future sessions.
- PIPro-DC
- Power graph is not correct when VRM's or Sinks are defined starting from pin definitions. All the other result data is correct. This issue does not occur when VRMs and sinks are defined from component instances.
- SIPro/PIPro, Via Designer
EM Simulation
- RFPro
- Project load fails with the error 'OccDesign::getNet: key not found' when a layout shape has a multi-bit net name (e.g. 'd<7:0>' or 'a,c,net1').
- With McAfee Endpoint Security (ENS) enabled, the Momentum surface current visualization hangs.
Workaround: Disable the "Enable Adaptive Threat Protection" flag in McAfee ENS. - DirectX 9 as graphics driver is no longer supported. DirectX 11 is thus used by default. Run "dxdiag" to verify which DirectX version is supported on your system.
If you run RFPro on a fresh machine with Suse 11 installed, you may encounter the critical error, "EMPro exited unexpectedly during execution."
Workaround: Run the following commands:cd $HPEESOF_DIR/fem/2020.00/linux_x86_64/bin
./startempro --personality=rfpro --driver=x11
Ignore any license related error messages that may show up on executing these commands. These driver settings are saved for future sessions.
- EM Setup
- On a Virtual Windows 10 system with Microsoft Hyper-V Video display driver, the 3D EM Preview with EM Setup Preprocessing may bring up a dialog with a Hoops error and, after suppressing the dialog, it opens up blank.
- Distributed simulations
The example implementation of the sitecluster command for LSF clusters may lead to failing simulations if path or number of threads is too large.
Workaround: See the workaround details in the sitecluster documentation.
Power Electronics
PowerMOS_SiC power devices operate under a very wide range of voltage and current slew rates and it is a challenge to create a model that converges under all conditions – especially conditions that depend upon what components are connected externally to the power device in the circuit schematic. Please contact technical support if you encounter such an issue when attempting to use this model.
If you run PEPro on a new machine with Suse 11 operating system, you may encounter the critical error, "EMPro exited unexpectedly during execution."
Workaround: Run the following commands:cd $HPEESOF_DIR/fem/2020.00/linux_x86_64/bin
./startempro --personality=pepro --driver=x11
You can ignore any license related error messages. These settings are saved for future sessions.
Installation
- While installing a new version of ADS, if you see “Previous version detected” error even after you have already run the uninstaller for that version of ADS, you may need to manually uninstall ADS before installation of the new ADS. To manually uninstall ADS, perform the following steps.
- Exit the current ADS installation session if it is running
- Remove or rename the file .com.zerog.registry.xml under the folder C:\Program Files\Zero G Registry . Both the folder and the file are by default hidden, so you may need to change the folder viewing setting to show hidden files and folders, do so via the Advanced settings of the View tab in the Windows Folder Options dialog box.
- Remove the ADS installation directory through the Windows Explorer.
- After performing the above steps, you can re-start the ADS installer.
Licensing
Unable to install Licensing Hardware Key Drivers on Windows.
Workaround: Turn off UEFI Secure Boot (BIOS) and use the default 6.3 version of the Wibu key driver delivered with the EEsof Licensing tools.Licensing may not support a license file path that is too long. This will likely occur when you have too many license files.
Workaround: Remove some license files, move the license files to a shorter directory path or to combine license files into a single file.License Setup wizard may not be able to start license server with many license files. During setup, it may lead to a situation where a command prompt window appears/disappears incessantly. This is due to the fact that License Setup wizard is not able to start lmgrd with a long command line and may get stuck in a loop.
Workaround:
- It is recommended to combine all license code words tied to same MAC ID into single license file to avoid setting large number of license files.
- Try to use a shorter path to place license files.
- If #1 and/or #2 does not help, start the license server (lmgrd.exe) from the command line (e.g. lmgrd.exe -c <lic-file-path> -l <license_server_log.txt>) and then set <PRODUCT>_LICENSE_FILE=<PORT-NUMBER>@localhost for product you want to use on same PC.
Dongle drivers for Flex-10 dongles on Linux are release specific. Installing the latest dongle drivers on Linux will function properly only for the most recent EEsof releases.
Workaround: Install and use dongle drivers as needed. If you need to run the most recent EEsof releases, use the latest Flex-10 dongle driver. If you need to use older releases, uninstall the latest dongle driver and re-install the older dongle driver- FLO and EEsof License setup are writing server logs at different locations. However, the EEsof server log file location is updated in the License Manager > Environment tab.
- When multiple same-named INCREMENT lines of different version exist on the license server, few advanced FlexNet options to reserve/limit licenses may not work properly.
- Product Selector “Check Availability“ generates incorrect results (which leads to license failure) for older releases when multiple date base versions of like-named bundles exist in the license pool.
- In Linux, Product Selector OK and Cancel Buttons locations are reserved.
- Starting from FlexNet Publisher 2015 (also known as version 11.13.1), the adoption of the best practice of the least-privilege security therein results in the License Server related Windows Service to run with the LocalService Account privilege (instead of the LocalSystem privilege as before.) Running with the LocalService Account privilege, an executable can no longer access any files located in the per-user specific type of folders. As a result, any license file placed in those folders can no longer be accessed by the License Server when the License Server is automatically started via the Windows Service upon each PC reboot. For the local node-locked license, this would not result in any disruption to the usage of EEsof applications; however, for the license installed on a network PC that is accessed by multiple client PCs, this may cause EEsof applications not to start after the network PC reboots
Workaround: Store your license files in the Windows folders that are accessible by the LocalService Account privilege. For example, C:\ProgramData or C:\users\public are both qualified choices. In general, any folder that has the "Users" group listed in its Properties > Security page and this "Users" group has the read permission enabled should work. Using the default port to connect to a license server may cause a delay when checking out licenses. If no port is given in the license file, Flexera scans ports 27000 to 27009 to find the port. Starting from FlexNet Publisher 2015 (aka version 11.13.1), the default timeout for the response from each port increased from .1 seconds to 3 seconds.
To avoid the delay, KSM now issues licenses with port 27009 instead of leaving this blank. The EEsof License Setup Wizard (from Licensing 2017.01 onwards) handles some common situations such as: where it detects license file(s) without port, when users get a new license file with port 27009, or when all license files for a vendor daemon does not have same port.
You will not be able to start the license server if all license files for a vendor daemon on a server does not have same port. Users who manually setup a license server or using EEsof License Setup Wizard with older licensing bits may need to manually edit license files to comply with the following rules:
All license files for a vendor daemon on a server must use the same port (or all be blank).
Using the default port (blank) is allowed but may result in longer checkout times.
If setting up a network server, select an unused port that is not blocked by a firewall.
Workaround: If the user cannot change the port, or wants to use the default Flexera ports, the environment variable FLEXLM_TIMEOUT can be set to .2 seconds (200000), to minimize the performance degradation. However, if the network latency is an issue in your environment, you may need to fine-tune this setting to minimize the general performance degradation while still accommodating the network latency.
- Installation of EESof EDA tools (such as, SystemVue 2016.08, Genesys 2017.XX, or ADS 2017.XX) may hang at 4% (percentage vary based on the products) for few hours or even more on some specific machines.
Workarounds:- Disable Firewall setting in Anti-Virus Software installed on the PC.
or - Download and unzip process explorer from the below link and then invoke procexp.exe.
https://technet.microsoft.com/en-us/sysinternals/processexplorer.aspx
Right click on the wusa.exe process under <Product installer exe> and select KillProcess. Now it will continue the product installation.
- Disable Firewall setting in Anti-Virus Software installed on the PC.
- After installing EESof EDA tools (such as, SystemVue 2016.08, Genesys 2017.XX, or ADS 2017.XX) successfully and try to invoke the software or License wizard, you may encounter “api-ms-win-crt-runtime-l1-1-0.dll” missing error.Workaround: Install the Update for Universal C Runtime in Windows . On Windows 64-bit system systems, the file to install is x64 version of the Microsoft hotfix KB2999226. A copy of the Windows6.1-KB2999226-x64.msu Microsoft 64-bit hotfix installer can be found under the
C:\Program Files\Keysight\EEsof_License_Tools\bin
directory. The Microsoft hotfix KB2999226 can be found under the Update for Universal C Runtime in Windows page at https://support.microsoft.com/en-us/help/2999226/update-for-universal-c-runtime-in-windows as well. - On a newly formatted RHEL system, the EEsof Licensing tools may fail to boot. This is because the FlexNet Publisher 2015 requires a certain rpm
Workaround: Under the EEsof product installation directory, there exists a utility script named "Linux_sys_check.sh" under the bin directory. Run this script to find out whether any rpm is missing; run this script with a "-y" command-line option to also have all the missing rpms automatically installed if you have the sudo or root privilege. - License server may stop recognizing Flex-10 dongle on some systems within a few hours after starting
Workaround: If you experience this problem, install the latest WibuKey drivers from Wibu Systems. - Unable to install Flex-10 driver if Flex-9 dongle is already plugged into a machine
Workaround: Before installing a Flex-10 driver for the first time, unplug the Flex-9 dongle. - There is a known FlexNet Publisher issue, whereby mixing node-locked codewords and floating codewords in one license file can result in: a) Remote simulations not working or b) A second local simulation not working in case the license is node-locked and also has incorrect version.
Workaround: It is strongly recommended that you do not mix node-locked codewords and floating codewords in one license file nor in any configuration that ends up with node-locked codewords and floating codewords both available on the same server. In other words, put the node-locked license and the floating license on different servers, and point to the respective one based on what you need to run. - If a user simultaneously runs two instances of a product and has mixed different versions of the same codeword on one license server, extra licenses may be pulled and result in unexpected “
Licensed number of users already reached for this feature
” errors.
Workaround: We recommend you remove expired codewords, to separate out the new and the old versions of codewords into different files and different servers, and to point to the respective one based on what you need to run. - Not specifying the TCP/IP port for the license server during license setup may lead to unexpected behavior and/or license checkout failure on the Windows platform. We strongly recommend you to always explicitly specify the TCP/IP port associated with each license server.
- A node-locked and floating bundle operating on Linux cannot be shared between products using EDA License Tools version older than 2014.01 when run at the same time.
- License Setup Wizard does not remove any previous user-configured FLEX Windows License Service manually set up by a user using FlexNet's lmtools.
Workaround: You must remove the previous user-configured Windows License Service via lmtools.Run the lmtools.exe from
C:\Program Files\Agilent\EEsof_License_Tools\bin
to invoke the lmtools utility. The lmtools utility window is displayed.If you have installed an EEsof product released before 1st August, 2014 on your system prior to installing an EEsof product released after 1st August, 2014 then the default EEsof Licensing tools path will remain C:\Program Files\Agilent\EEsof_License_Tools.
On the systems that only have EEsof products released after 1st August, 2014 installed then the default EEsof Licensing tools path will beC:\Program Files\Keysight\EEsof_License_Tools.
- In the Service/License File tab, check the Configuration using Services option. All user-configured FLEX Windows License Services will be listed.
- Select the service you wish to remove.
- Select the Config Services tab and click the Remove Service button to remove the service.
To ensure that the license service or lmgrd is running, click View Log. A log window appears that confirms whether agileesofd and lmgrd are up and running.
- While running multiple versions of prior ADS releases together, set ADS_MAXIMUM_BUNDLE_USAGE=ON in your environment so that all of them will use the same method to check out licenses. Otherwise, you might receive an error message, "Licensed number of users already reached".
- On some Windows 7 machines, when more than one definition of an Ethernet adapter exists (duplicates), license checkouts may appear to hang up.
Workaround: Disable the duplicate network card definitions in your network settings: Control Panel > Network and Internet > Network Connections. This issue has been acknowledged by Flexera and they have created a bug report (SIOC-000103097). - For LSF style distributed simulations, ensure that the PATH on the client computer points to the $HPEESOF_DIR/EEsof_License_Tools/${architecture} directory that corresponds to the EEsof release being used. This needs to be done in order to ensure that the proper version of the Flexera utilities (like lmutil ) gets picked up in the path before any older in-compatible versions (that may also be installed on a users’ system.)
- License Setup Wizard ( aglmwizard.exe ), which is used to set up and record the license path would not work if you already have an environment variable set for ADS_LICENSE_FILE.
Workaround: You can use ADS_LICENSE_FILE variable to point to license file or refer to Licensing (For Administrators). - The License Setup Wizard will exit or not properly configure a license server, if the server has all of its licenses currently in use.
Workaround: Wait for a license on the server to become available as you normally would before launching the product. - Unable to set license in case unicode characters are used either in path or license file name because the Flex License Service does not support these characters.
The Product Selector tool will be unable to display the license server status properly when connected to older license server.
Workaround: Upgrade your license server to the latest version.EEsof Licensing Tools installer can hang on systems with McAfee LiveSafe installed and running the default firewall settings.
Workaround: Prior to installing EEsof Licensing Tools, temporarily turn off the McAfee LiveSafe firewall.Licensing setup steps on systems with McAfee LiveSafe installed can fail.
Workaround: Under the McAfee LiveSafe firewall settings, under Port and Settings, allow the use of port 27001 for lmgrd.exe under the EEsof Licensing Tools installation bin directory. Under Internet Connections for Programs , enable lmgrd.exe, aglmmgr.exe and aglmwizard.exe for all devices and turn off monitoring.- On Windows, EEsof product releases prior to 2014 can have boot time issues with licensing if an newer EEsof product is installed prior to installing the older product. For example, if a users installs Advanced Design System 2017 and then installs Advanced Design systems 2014.01, the user can have boot time errors with ADS 2014.01.
Workaround: For Advanced Design System users, set a system environmental variable named ADS_LICENSE_FILE under the Control Panel/ System, and Security / System / Advanced system settings and under the "environmental variables". Add an System variable named ADS_LICENESE_FILE and the value will be the path to your local license file or the port@host setting for your site.
Third Party Applications
- Spyder application menu bar becomes inactive when the window is maximized using View > Full Screen or by pressing F11 (shortcut key to maximize the screen).
Workaround: Press F11 again to make it the default screen. The menu bar is now active and works fine.
Verification Test Bench
Run the following command parameter. Where, VTB_Examples.wsv is old SystemVue file and VTB_examples_new.wsv is converted file. The following successful message is displayed. You can now use the VTB_examples_new.wsv workspace in ADS.
Workaround: You need to manually uninstall VTB from Start > Control Panel > Add/Remove Program.
In ADS, the customized VTB can have the backward compatibility issue.
Workaround: To fix this issue, use one of the following method:C:\ADS_VTB>"<ADS_Install_Dir>\SystemVue\2018\ win32_64\ bin\ WorkspaceConversionTool.exe" VTB_Examples.wsv VTB_examples_new.wsv
Created: VTB_example_new.wsv
Examples - Known Issues
Examples under <ADS Install Directory>\examples \Instrument_links folder are not getting opened on Linux where as they are opening fine on Windows.
Workaround: Rename the ‘Instrument_links’ folder to ‘Instrument_Links’, if you have write permission to the <ADS Install Location>\examples folder. In case you do not have the write permission then proceed with manual unarchive process (File > Unarchive from the ADS Main window) pointing to the Example workspace.Example search might not work and prompt you the "Database is locked" error when ADS installation is on NAS.
Workaround: Restart the nfslock service on client. In case the problem still persists, reboot the client to unlock the database.
- Unable to compile Pin Diode Model using Visual Studio 2012 on Windows 7 64-bit platform.
Workaround: Delete the contents of the directory examples\RF_Microwave\UserCompiledModel_wrk\UserCompiledModel\lib.win32_64
before using UCMs. - An error occurs while running a custom VTB.
Workaround: Download and run a custom VTB from the following location: <ADS Install Location>\SystemVue\2016.08\win32_64\VTB.
Documentation
On Windows, Printing directly from installed help generates non-readable output.
Workaround: Use PDF version of the document for printing purpose.From ADS 2016.01 onwards, in ADS help when you open a page using the "Open a link in new tab" option the help does not open a page in a different tab by default. You need to set the preferences to open any link in a new tab.
To set the preferences:From the ADS 20xx (or the installed version) Help, Click File > Edit > Preferences.
The Preferences Dialog box is displayed.Select the Options tab.
Under Appearance, select the Show tabs for each individual page option.
- Unable to open online help, any external link, or Embedded Survey link in Linux on Mozilla Firefox browser.
Workaround: Use Mozilla Firefox version 39 or above or keep the Firefox window open and then try to open online help. - While using the installed ADS help, you may encounter issues like help not showing any content, it throws an error, it displays unexpected hierarchy in the Content tab, or it does not display any search results.
Workaround: Close the help, delete the contents of the following directory and open the help again.- On Windows:
C:\Users\<Windows_Login_ID>\AppData\Local\Keysight\Help
- On Linux:
$HOME/.local/share/Keysight/Help
- On Windows:
- ADS installed help search does not support [] or {} or any other text using these combinations.