Here’s the page we think you wanted. See search results instead:

 

  

Main Support:       Knowledge Center
Documentation:   SystemVue English Doc   >  sv201608   >  SystemVue 201608 Quick Install and License Setup   >  SystemVue 201608 Quick Install and License Setup

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Comment: Migration of unmigrated content due to installation of a new plugin
Scroll Ignore
HTML
<!--start_panel_strip-->
Float
bordernone
sideright
width25%
Panel
borderColor#eaeef6
bgColor#eaeef6
borderStylesolid

On This Page

Table of Contents
maxLevel3
indent15px
HTML
<!--end_panel_strip-->

gloss_init

Scroll Ignore

Quick Install and License Setup

SystemVue can be installed on a Windows machine after downloading the installation file from the Keysight EEsof EDA website, as illustrated.

Anchor
WinFlowchart
WinFlowchart

                       

Scroll ImageMap
viewSize0.0
imgWidth0.0
areasData{"areas":[{"shapeType":"rect","coords":"74.0,23.0,122.0,10.0","linkTarget":"_self"},{"shapeType":"rect","coords":"76.0,112.0,178.0,35.0","linkTarget":"_self"},{"shapeType":"rect","coords":"291.0,124.0,113.0,9.0","linkTarget":"_self"},{"shapeType":"rect","coords":"426.0,124.0,120.0,11.0","linkTarget":"_self"},{"shapeType":"rect","coords":"32.0,192.0,222.0,49.0","linkTarget":"_self"},{"shapeType":"rect","coords":"298.0,215.0,255.0,15.0","linkTarget":"_self"},{"shapeType":"rect","coords":"27.0,286.0,228.0,54.0","linkTarget":"_self"},{"shapeType":"rect","coords":"86.0,405.0,100.0,10.0","linkTarget":"_self"}]}
imgRelativeInstallFlowChart.png
meta{"missingImgDimensions":true}
imgHeight0.0
alwaysHighlightfalse
dataModelVersion3

Anchor
ObtLic
ObtLic

Obtain SystemVue License File

SystemVue requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer. For example, you can save it in the C:\Program Files\Keysight\EEsof_License_Tools\bin\licenses folder.

Anchor
supplatform
supplatform

Supported Platforms

For details on the supported platforms, see Supported Platforms.

Anchor
SysReqWnd
SysReqWnd

System Requirements

The following list the recommended hardware configuration. For detailed system requirements, see System Requirements.

Category

 

Practical Minimums

 

Recommended Basic

 

Recommended 5G, Radar, and Phased Array

Operating System

 

Windows 7 SP1, 64-bit

 

Windows 10, 64-bit

 

Windows 10, 64-bit

CPU

 

Single-core

 

Quad-core and above

 

Quad-core and above

Hard disk

 

10 GB free space

 

100 GB free space

 

100 GB free space

RAM

 

4 GB RAM

 

16 GB RAM and above

 

32 GB RAM and above

Display

 

1280 x 720

 

1920 x 1200

 

1920 x 1200

Software Security

 

USB hardware key

 

Wired LAN, or Wireless LAN

 

Wired LAN, or Wireless LAN

LAN Connection

 

Not required

 

Recommended

 

Recommended

Test Instrument Interface

 

Not required

 

LAN

 

LAN

Touch User Interface

 

N/A

 

Not supported

 

Not supported

Anchor
svDldPg
svDldPg

Download SystemVue Installer

Click http://www.keysight.com/find/eesof-systemvue-latest-downloads to download. You can also use Keysight Download Manager to download.

Anchor
windowsgeneralinstallation
windowsgeneralinstallation

Install SystemVue

To install SystemVue, you must have system administrator privileges. Run the downloaded installer (this may take a while). Follow the guided tour to complete the installation.

Anchor
SVLicSetup
SVLicSetup

SystemVueLicense Setup

At the end of the installation, the License Setup Wizard starts automatically when it detects that you do not have a valid license to start SystemVue. If you choose to skip the setup, you can start the SystemVue License Setup Wizard later by clicking Start > All Programs > SystemVue <release_number> > SystemVue Tools > SystemVue <release_number> > License Manager.

Nodelocked License

Choose the I want to add or replace a license file option and follow the guided tour to complete the license setup process.

Lp_note

In the case of a USB dongle, attach the dongle to the USB port and invoke the License Setup Wizard to take the guided tour.

Floating License

Choose the I want to add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server. For more details on setting up floating license on a network server, see Setting Up Floating License on Windows.

Anchor
launchsv
launchsv

Launch SystemVue

To run SystemVue, go to the Start menu and choose All Programs > SystemVue <release_number> > SystemVue <release_number>

Lp_note

On Win8 platform, if you see a "Windows Features" dialog window asking for installation of .NET Framework 3.5 , please do "Download and install this feature". For more information, please visit: http://msdn.microsoft.com/en-us/library/bb822049.aspx

 

 

Scroll Ignore

 

 

Scroll Ignore
 
Please help us improve
Please help us improve
Was this topic helpful? Yes No