Here’s the page we think you wanted. See search results instead:

 

  

Main Support:       Knowledge Center
Documentation:   SystemVue English Doc   >  sv2020update1   >  PathWave System Design (SystemVue) 2020 Update 1.0 Quick Install and License Setup   >  PathWave System Design (SystemVue) 2020 Update 1.0 Quick Install and License Setup

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Comment: Migration of unmigrated content due to installation of a new plugin
Scroll Ignore
HTML
<!--start_panel_strip-->
HTML
<!--end_panel_strip-->

gloss_init

Scroll Ignore

PathWave System Design (SystemVue) Quick Install and License Setup

PathWave System Design (SystemVue) can be installed on a Windows machine after downloading the installation file from the Keysight EEsof EDA website, as illustrated.

Anchor
WinFlowchart
WinFlowchart

                       


Anchor
ObtLic
ObtLic

Obtain PathWave System Design (SystemVue) License File

PathWave System Design (SystemVue) requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer. For example, you can save it in the C:\Program Files\Keysight\EEsof_License_Tools\bin\licenses folder.

Anchor
supplatform
supplatform

Supported Platforms

For details on the supported platforms, refer to Supported Platforms.

Anchor
SysReqWnd
SysReqWnd

Download PathWave System Design (SystemVue) Installer

Click http://www.keysight.com/find/eesof-systemvue-latest-downloads to download. You can also use Keysight Download Manager to download.

Anchor
windowsgeneralinstallation
windowsgeneralinstallation

Install PathWave System Design (SystemVue)

To install PathWave System Design (SystemVue), you must have system administrator privileges. Run the downloaded installer (this may take a while). Follow the guided tour to complete the installation.

Anchor
SVLicSetup
SVLicSetup

PathWave System Design (SystemVue) License Setup

At the end of installation, the License Setup Wizard starts automatically when it detects that you do not have a valid license to start PathWave System Design (SystemVue). If you choose to skip the setup, you can start the SystemVue License Setup Wizard later by clicking Start > All Programs > SystemVue <release_number> > SystemVue Tools > SystemVue <release_number> > License Manager.

Nodelocked License

Choose the I want to add or replace a license file option and follow the guided tour to complete the license setup process.

Lp_note

In case of a USB dongle, attach the dongle to the USB port and invoke the License Setup Wizard to take the guided tour.

Floating License

Choose the I want to add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server. For more details on setting up floating license on a network server, see Setting Up Floating License on Windows.

Anchor
launchsv
launchsv

Launch PathWave System Design (SystemVue)

To run PathWave System Design (SystemVue), go to the Start menu and choose All Programs > SystemVue <release_number> > SystemVue <release_number>






Please help us improve
Please help us improve
Was this topic helpful? Yes No