Here’s the page we think you wanted. See search results instead:

 

  

Main Support:       Knowledge Center
Documentation:   Genesys English Doc   >  genesys2020   >  Genesys 2020 Quick Install and License Setup   >  Genesys 2020 Quick Install and License Setup

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Comment: Migration of unmigrated content due to installation of a new plugin


gloss_init

Scroll Ignore

Quick Install and License Setup

Genesys can be installed on a Windows machine after downloading the installation file from the Keysight EEsof EDA website, as illustrated.

Anchor
WinFlowchart
WinFlowchart

                       


Anchor
ObtLic
ObtLic

Obtain Genesys License File

Genesys requires a license to run. You can either apply for an Evaluation or a Purchased license. Once the license request is approved, a license file (with .lic extension) is sent as an email attachment. Save this file on your computer. For example, you can save it in the C:\Program Files\Keysight\EEsof_License_Tools\bin\licenses folder.

Anchor
supplatform
supplatform

Supported Platforms

For details on the supported platforms, refer to Supported Platforms.

Anchor
SysReqWnd
SysReqWnd

System Requirements

The following list the recommended hardware configuration. For detailed system requirements, see System Requirements.


Category

Practical Minimums

Recommended or Typical

Operating System

Windows 7 (64-bit), Windows 10 (64-bit)

Windows 10 (64-bit)

CPU

Dual-core

Quad-core or above

Hard disk

10 GB free space

100 GB free space

RAM

6 GB RAM

32 GB RAM

Display

1920 x 1080

1920 x 1200

Software Security

USB hardware key

Wired LAN, or Wireless LAN

Internet Connection

Not required, but USB/DVD drive needed for SW updates

Highly recommended

Test Instrument Interface

Not required

LAN

Touch User Interface

N/A (Windows 7), Not supported (Windows 10)

N/A

Download Genesys Installer
Anchor
svDldPg
svDldPg

Click http://www.keysight.com/find/eesof-genesys-latest-downloads to download. You can also use Keysight Download Manager to download.

Anchor
windowsgeneralinstallation
windowsgeneralinstallation

Install Genesys

To install Genesys, you must have system administrator privileges. Run the downloaded installer (this may take a while). Follow the guided tour to complete the installation.

Anchor
SVLicSetup
SVLicSetup

Genesys License Setup

At the end of installation, the License Setup Wizard starts automatically when it detects that you do not have a valid license to start Genesys. If you choose to skip the setup, you can start the Genesys License Setup Wizard later by clicking Start > All Programs > Genesys <release_number> > Genesys Tools > Genesys <release_number> > License Manager.

Nodelocked License

Choose the I want to add or replace a license file option and follow the guided tour to complete the license setup process.

Lp_note

In case of a USB dongle, attach the dongle to the USB port and invoke the License Setup Wizard to take the guided tour.

Floating License

Choose the I want to add or replace a network license server option and follow the guided tour to complete the license setup process. Consult your license administrator for the network path of the license server. For more details on setting up floating license on a network server, see Setting Up Floating License on Windows.

Anchor
launchsv
launchsv

Launch Genesys

To run Genesys, go to the Start menu and choose All Programs > Genesys <release_number> > Genesys <release_number>

Please help us improve
Please help us improve
Was this topic helpful? Yes No