Here’s the page we think you wanted. See search results instead:

 

  

Main Support:       Knowledge Center
Documentation:   EMPro English Doc   >  Previous Supported Releases   >  EMPro 2019   >  EMPro 2019 Release Notes   >  EMPro 2019 Release Notes

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  • To facilitate the creation of parameterized objects during sketching, the default solve mode for the constraint manager is now the XY plane. In a python script, you can change the solve mode to full 3D by the following command: sketch.constraintManager().solveMode='XYZ'
  • The import HFSS (.aedt/.a3dcomp + .sat) has been improved.
  • The 'python_scripts/demo/commandline/run_simulation.py' script that demonstrates how you can create and run a new simulation from the command line has been updated to support parameter sweeps.

Licensing

...

  • EMPro 2019 requires: a) the version 2018.04 of the EEsof EDA licensing software, b) a minimum code-word version 2018.04 or above, and c) the licensing server software, lmgrd and agileesofd, to be upgraded to at least the same versions as what are included in EEsof EDA Licensing software 2018.04. EMPro 2019 will not start if any of these requirements is not met. Refer to the License Codeword Version Compatibility Table.
  • In the EEsof EDA License Tools version 2018.04, licensing vendor daemon (agileesofd) is integrated with FlexNet FNP 11.13.1.4 version (Windows) and FlexNet FNP 11.13.1.3 version (Linux) of FlexNet license manager daemon (lmgrd). For the Windows platform, EMPro installer will automatically set up these two new license server daemons by default for the local node-locked license users; for the Linux platform, you need to follow the Setting Up Licenses on Linux instruction to complete the licensing configuration process. For more details, refer to Licensing (For Administrators).

Known Issues and Solutions

...

Please help us improve
Please help us improve
Was this topic helpful? Yes No