Skip to end of metadata
Go to start of metadata

Supported Platforms

The following table lists the supported platforms for GoldenGate.

Operating System and Version

RedHat Linux RHEL6

RedHat Linux RHEL7RedHat Linux RHEL8

Suse Linux SLES11

Suse Linux SLES12

GoldenGate 2017

GoldenGate 2020/2020 Update 1.0

GoldenGate 2022

GoldenGate 2022 Update 1.0


For information on previous GoldenGate releases, see GoldenGate Supported Platforms for Previous Releases.




Legend

Description

Supported

Unsupported