License Setup through Wizard
This section describes how to setup your EMPro license using EMPro License Setup Wizard. The License Setup Wizard helps you to set up your local node-locked license on PC, or to point to an already configured network license server. It can be used to setup EMPro licenses for following scenarios:
- EMPro 2011 only: If you are using only EMPro 2011 (and not previous versions), you can complete the license setup by using this wizard.
- Multiple
EMPro versions
- Each EMPro version having its own License: If you are using multiple EMPro versions and you have individual license for each EMPro version, you can still complete the license setup by using License Setup Wizard.
- All
EMPro versions are using new license version 2.9: If you are using multiple
EMPro versions
EMPRO_LICENSE_FILE
- You may receive a dual license file which contains both 2.9 counted codewords as well as 2.8 uncounted codewords for the same feature. You can use any of the following options for this type of dual license setup:
- Sharing method: Set it up using
EMPro License Setup Wizard, and modify
AGILEESOFD_LICENSE_FILE
to@localhost
to share the license server running in the background. - Simple method: Copy the the combo license file to the
licenses
sub-folder of your EEsof product installation tree.
- Sharing method: Set it up using
EMPro License Setup Wizard, and modify
- Multiple EEsof Products: If you are using more than one EEsof products, you can use product specific license wizard to complete the license setup.
- EEsof and other Agilent or EDA Products: If you are using other Agilent products or EDA products (along with EEsof products), you can still use EEsof product specific license wizard to complete the license setup. For license setup of other Agilent or EDA products, refer to their product documentation.
Note
For latest updates, click here to refer online version of this document.
License Setup Wizard
EMPro License Setup Wizard is a new tool that simplifies the license setup. This wizard helps you to set up your EMPro license. This wizard can be used in all previously discussed scenarios with some manual changes, in case all EMPro version are using license version 2.9. The wizard provides an easy method to:
- Add or replace license files
- Add or replace license servers
- Request additional licenses
You can apply for evaluation license or apply to purchase a new license.
Important
- Before setting up your
EMPro license, you must obtain the new
EMPro license version 2.9. License version prior to 2.9 will not work with latest
EMPro
- To start the license server manually, you must use the latest version of license utilities (such as, lmtools, agileesofd, and lmutil). These utilities can be accessed from:
-
- Windows:
C:\Program Files\Agilent\EEsof_License_Tools
folder - Unix (32 bit):
<install_folder>/EEsof_License_Tools/linux_x86
- Unix (64 bit):
<install_folder>/EEsof_License_Tools/linux_x86_64
- Windows:
-
- If you install multiple EEsof products or install EMPro several times on a single system, the EEsof license tools directory will already exist and you will not be prompted for a location for these files. A single EEsof license tool installation will support multiple EEsof products and multiple releases of EMPro.
Evaluation License
If your request for EMPro evaluation license is approved, you will receive a license file (of EMPro license version 2.9) as an attachment through e-mail. Save this license file on your computer as EMPro License Setup wizard need this file to complete the license setup.
Purchased License
If you have purchased the EMPro license, you will receive your license file as an attachment through e-mail. The license file can be saved in any convenient location. The License Setup Wizard will be used to locate and add the license file to the license server.
Starting License Setup Wizard
After successful installation of the product, the interactive License Setup wizard starts automatically. This interactive wizard searches for valid EMPro licenses. If any valid EMPro license is found, the license setup wizard confirms the same with a message and you can launch EMPro. Otherwise, wizard displays a "Cannot Find a License for this Product" message along with options to setup the licenses (if you have already purchased) or submit the request for a new license.
Note
To manually start the License Setup wizard,
- Windows: Choose
EMPro 2011.04 > EMPro Tools > EMPro 2011.04 License Setup Wizard
- Unix: Run
aglmwizard
from<install_folder>/EEsof_License_Tools/linux_x86
folder.
- Unix: Run
Three options displayed by License Setup Wizard are:
- I want to request a license file: Select this option if you want to submit online request to receive a license file.
- I have a license file to install: Select this option if you have already received a license file and ready to setup.
- I want to add or replace a license server: Select this option if you want to access the license from a server.
Note
For information about License File and License Server, click on the links provided in the License Setup Wizard.
Request New License File
Follow the steps below to submit a request for a new license file (evaluation or purchase):
- Choose Programs >
EMPro 2011.04 > EMPro Tools > EMPro 2011.04 License Setup Wizard
Note
License Setup Wizard starts automatically if EMPro is launched and there are issues with license setup.
- Select I want to request a license file or I want to request additional licenses and click Next.
- Select I want an evaluation license to submit request for an evaluation license of
EMPro or I want to get my purchased licenses to submit request for new purchase and click Next. If you select I want to get my purchased licenses then skip the next three steps.
- To receive an evaluation license select I have an evaluation token if you already have the token to receive evaluation license. Otherwise, select I want to apply for an evaluation license.
- Click Next.
- From Request Evaluation License screen, click Agilent EEsof EDA Evaluation License Request Form and submit online request for your license.
- If you selected I want to get my purchased licenses option, click Agilent Software Manager and submit online request for your license.
- Click Finish to terminate the wizard.
Note
If your evaluation license request is approved, you will receive the license file of EMPro license version 2.9.
License File Setup
If you have received email with attached license file (file with extension .lic
), save the file on your computer (for windows, preferred locations is C:\Program Files\Agilent\EEsof_License_Tools
and for Unix, <install_folder/EEsof_License_Tools
folder)
- Start the License Setup Wizard (as described in previous steps).
Note
The license wizard starts automatically if you launch EMPro without completing the license setup.
- Select I have a License file to install and click Next.
- To add the license file, click Add and navigate to the location where license file is located.
Note
License file can be placed anywhere on the system. Agilent recommends you to copy the license file in
C:\Program Files\Agilent\EEsof_License_Tools
for windows. - Click Next. On successful license setup, a confirmation message (see figure below) is displayed.
Note
If you want to perform additional license tasks like add or replace a license file, add or replace a license server, or request additional licenses then select I want to perform additional licenses tasks and click Next.
- Click Exit to terminate the wizard.
Note
You can add multiple license files separated by semicolon (;).
License Server Setup
Follow the steps below to access the license from a server:
- Start the License Setup Wizard (as described in previous steps).
The license wizard starts automatically if you try to launch EMPro without completing the license setup.
- Select I want to add or replace a license server and click Next.
- To add a license server, enter the server name and click Next. A confirmation message is displayed on successful setup of the license.
Note
If you want to perform additional license tasks like add or replace a license file, add or replace a license server, or request additional licenses then select I want to perform additional licenses tasks and click Next.
- Click Exit to terminate the wizard.
Note
You can add multiple license server names separated by a semicolon(;).
Add/Upgrade your License File
To add new licenses or upgrade your existing Evaluation License to Purchased License, follow the steps below:
- Choose Programs >
EMPro 2011.04 > EMPro Tools > EMPro 2011.04 License Setup Wizard or click
- Click Next to start the license setup process.
- In License Status screen, select I want to add or replace a license file and click Next.
- To add a new license file or replace an existing license file, click Add and select the license file to be added or replaced with existing license.
Note
You can add multiple license files.
- Click Next. A confirmation message is displayed after successful setup of license.
License Setup for Previous EMPro Releases
To use license version 2.9 or later, for previous EMPro releases
, you must manually change the environment variable setting. There are different ways to change those settings and two commonly used options are listed below.
Using Registry Editor
You can use registry editor to set the
EMPRO_LICENSE_FILE
Environment Variable settings
If you are using license version 2.9 for previous EMPro releases
, you must manually add the environment variable
EMPRO_LICENSE_FILE
. This variable must point to the license file (along with file name and location).